FAQ
FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Low-voltage Circuit Breakers > Air Circuit Breakers > ACB drawout position
FAQ
ACB drawout position
Which drawout positions are there for Drawout type?
Answer
Drawout type circuit breaker can be drawn-out and insert to the cradle without taking out the connecting conductor. As ACB is drawn out, it will be "connect position" , "Test position" (main circuit is disconnected and only control circuit is connected) and "Disconnect position" (both main circuit and control circuit are disconnected)
- Product Name
- Low Voltage Air Circuit Breakers
- Series
- AE-SW