Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22433
  • Release Date : 2018/08/31 14:33
  • Print

Fixed-type and Adjustable-type of V-type Operating handle

What is the difference between Fixed-type and Adjustable-type of V-type Operating handle?
Category : 

Answer

For Fixed type, the depth from the circuit breaker mounting surface to the panel board front is fixed. Adjustable-type is used when the depth from the circuit breaker mounting surface to the panel board front is deeper than Fixed type. It can be adjusted by cutting the shaft.(Max 300mm)
Product Name
External Accessories
Series
WS-V

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries