FAQ
FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Low-voltage Circuit Breakers > Molded Case Circuit Breakers > Degree of protection
FAQ
Degree of protection
What does "degree of protection" mean?
Answer
In order to prevent breakdowns and human injuries, it is necessary to select a control device having protection structure suitable for each purpose. The protection class of the control devices is called "degree of protection". This can be classified depending on the structure for human body and protection against water intrusion etc.
- Product Name
- Molded Case Circuit Breakers
- Series
- WS-V