FAQ
FAQAbout Products
- FAQ > Robots > Industrial/Collaborative Robots-MELFA > Vertical type robot > An unusual noise can be heard (from RC).
FAQ
An unusual noise can be heard (from RC).
An unusual noise can be heard (from RC).
Answer
Cause:
- A noise is made as the internally mounted fan and its casing resonate.
- A noise is made by the fan catching internal wiring.
Measures:
- Check the state of the cover fastening.
- Check to see whether or not the fan is interfering with cables, etc.
- Product Name
- Industrial Robots MELFA
- Series
- FR Series
F Series