Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23170
  • Release Date : 2018/09/07 16:09
  • Print

The servo-on cannot be performed.

Answer

Cause:

  • A servo OFF signal(SRVOFF)is being input from an external source.
  • The operating right is not given.(IOENA parameters settings/exclusive input and output).
  • An error is occurring.
  • TB operation error(enabling switch, activate/deactivate)

Measures:

  • Check for a servo OFF signal and check the operation rights.
  • Check how to operate the TB. Check that the 3 position enabling switch is set to the middle position.
  • If an error message is occurring please cancel it.

Product Name
Industrial Robots MELFA
Series
FR Series
F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?