Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23174
  • Release Date : 2018/09/07 16:09
  • Print

Oil is leaking.

Answer

Cause:

  • Deterioration in the reducer oil seal.
  • Too much grease was applied.
  • A grease other than the specified grease was applied.
  • Excess grease left on the unit when grease was applied.
  • Foreign materials have stuck to the oil seal(dust, etc.).

Measures:

  • Check the amount of grease that should be applied and the name and product number of the grease.
  • Take measures to make sure that dust, etc. does not adhere to joints.
  • After applying grease wipe off any grease that is protruding.

Product Name
Industrial Robots MELFA
Series
FR Series
F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?