Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23175
  • Release Date : 2018/09/07 16:09
  • Print

Breaker trips/overcurrent error occurs.

Answer

Cause:

  • Deterioration in the packing.
  • Scaling on the packing.
  • Using a highly permeable cutting oil.
  • An environment that exceeds the IP functionality.

Measures:

  • In a mist environment, pull off and replace the packing every time the cover is removed.
  • If a highly permeable cutting fluid is being used, or in an environment that exceeds the IP functionality, purge the air and take measures on the jacket.
* Cutting oil that has got inside the arm must be thoroughly cleaned away or the components inside the arm are at risk of rotting.

Product Name
Industrial Robots MELFA
Series
FR Series
F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?