Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23176
  • Release Date : 2018/09/07 16:09
  • Print

The hand does not move properly (air hand).

Answer

Cause:

  • An air leak/break in the piping.
  • The solenoid bulb has failed.
  • Wire breakage on the hand signal line.
  • Hand signal line short circuit
  • The hand IF card has failed or has been inserted incorrectly.
  • Sink/source setting error.
  • Hand connecting wire error
  • Insufficient air pressure.
  • A foreign material has got stuck in the air hose.
  • Faulty connection in the cables that run between devices.

Measures:

  • Carry out a check on the air hose, joints, air pressure, and connecting wire.
  • Check the condition of the hand input/output signal.
  • Check whether or not the controller's sink/source settings and wiring are consistent with each other.
  • Check the condition of the connections on the cables that run between devices.

Product Name
Industrial Robots MELFA
Series
FR Series
F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?