Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23178
  • Release Date : 2018/09/07 16:09
  • Print

Brake is not working properly.

Answer

Cause:

[Occurs only when operating manually]
•T/B operation error.
[Occurs when operating manually and automatically]
•Faulty connection of the cables that run between devices.
•Brake failure.

Measures:

[Occurs only when operating manually]
•Check the T/B operation(operation buttons, 3 position enabling switch, etc.).
[Occurs when operating manually and automatically]
•Check the mating of the cables that run between devices.

Product Name
Industrial Robots MELFA
Series
FR Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?