FAQ


FAQAbout Products
- FAQ > Robots > Industrial/Collaborative Robots-MELFA > Vertical type robot > The communication fault occurs by the equipment connected to the Ethernet cable inside the robot arm.
FAQ
The communication fault occurs by the equipment connected to the Ethernet cable inside the robot arm.
The communication fault occurs by the equipment connected to the Ethernet cable inside the robot arm.
Answer
Cause:
- The Ethernet cable is not connected surely.
- There are the device etc. which cause the noise and the noise has applied to the Ethernet cable.
Measures:
- Confirm that the Ethernet cable is connected surely.
- If the effect by the noise can be considered, find out the noise source and remove the noise. Moreover, adds the grounding and ferrite core of the Ethernet cable if needed.
- Product Name
- Industrial Robots MELFA
- Series
- FR Series
F Series