Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23184
  • Release Date : 2018/09/07 16:09
  • Print

The T/B does not display anything.

Answer

Cause:

  • The fuse (4A fuse) installed at the bottom of the 24 V power supply circuit in the controller may have blown out.
    For the fuse blowout, the emergency stop made by the customer may be the cause, or there may be a ground fault or short circuit with the 24 V power supply in the wiring of a door switch, enabling device, etc.
  • The T/B might be out of order.

Measures:

  • Investigate and correct the ground fault or short circuit portion in the wiring made by the customer. Then, replace the fuse inside the controller.

Product Name
Industrial Robots MELFA
Series
F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries