FAQ


FAQAbout Products

- FAQ > Low-voltage Power Distribution Products > Contactors and Motor Starters > Motor Starters > About Low-voltage Power Distribution Products
FAQ
About Low-voltage Power Distribution Products
How should I connect MSO-T* and MSO-N* type magnetic starterwhen using for opening/closing single-phase motor load?
Answer
Since it is necessary to energize the pole containing a heater element of athermal load relay, you need to connect it to both side of 3 poles(Between 1/L1-2/T1 and between5/L3-6/T3).
- Product Name
- Motor Starters
- Series
- MS-T/N