FAQ
FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Contactors and Motor Starters > Motor Starters > About Low-voltage Power Distribution Products
FAQ
About Low-voltage Power Distribution Products
Is it possible to use surge suppressor unit UT-SA33* or UN-SA33type for a main circuit in a single-phase?
Answer
It is possible to apply for single-phase circuit. However, it may be lesseffect in single-phase circuit (100 V, etc) since low voltage circuit is tendedto be less effect.
- Product Name
- Motor Starters
- Series
- MS-T/N