FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Low-voltage Power Distribution Products > Contactors and Motor Starters > Motor Starters > About Low-voltage Power Distribution Products
FAQ
About Low-voltage Power Distribution Products
What are the minimum applicable voltage and current of SR-T* andSRD-T* type contacts?
Answer
The minimum applicable load is 20V, 3mA . Contact reliability is indicatedby fault rate λ60 (Number of fault / Operating cycles per one contact) atthe reliability level 60%. = 1*10-7 / time
- Product Name
- Motor Starters
- Series
- MS-T/N