Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23335
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

Is it possible to install S-T* and S-N* type by rotating 90℃ to theright or left from the regular installation?
Category : 

Answer

It is possible to install them by rotating 90℃ to the right or left from theregular installation except S-N600 and S-N800. It is not possible to rotate180℃ for all of them.
Product Name
Motor Starters
Series
MS-T/N

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries