FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Using the devices connectable to the GOT1000 series
FAQ
Using the devices connectable to the GOT1000 series
Can the devices connectable to the GOT1000 series be used with the GOT2000 series?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21
Answer
The devices connectable to the GOT1000 series can be used with the GOT2000 series as well.
However, some optional devices cannot be purchased due to discontinuation of production. In such a case, please change the equipment configuration or connection type (for example, changing A-bus connection to direct CPU connection).
For the details, refer to the following.
・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
・ GOT2000 Series Connection Manual (Non-Mitsubishi Electric Products 1) For GT Works3 Version1 (SH-081198ENG)
・ GOT2000 Series Connection Manual (Non-Mitsubishi Electric Products 2) For GT Works3 Version1 (SH-081199ENG)
・ GOT2000 Series Connection Manual (Microcomputers, MODBUS/Fieldbus Products, Peripherals) For GT Works3 Version1 (SH-081200ENG)
However, some optional devices cannot be purchased due to discontinuation of production. In such a case, please change the equipment configuration or connection type (for example, changing A-bus connection to direct CPU connection).
For the details, refer to the following.
・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
・ GOT2000 Series Connection Manual (Non-Mitsubishi Electric Products 1) For GT Works3 Version1 (SH-081198ENG)
・ GOT2000 Series Connection Manual (Non-Mitsubishi Electric Products 2) For GT Works3 Version1 (SH-081199ENG)
・ GOT2000 Series Connection Manual (Microcomputers, MODBUS/Fieldbus Products, Peripherals) For GT Works3 Version1 (SH-081200ENG)
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (communication), supported model (controller)
- Series
- GOT2000 Series