FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > VNC server function trial
FAQ
VNC server function trial
Can I try the VNC server function without the license of the VNC server function (for the GOT2000 series)?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21
Answer
You can try the VNC server function up to 30 times in total (up to 15 hours) by counting one continuous use within 30 minutes as one time.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (VNC server), license (VNC server)
- Series
- GOT2000 Series