FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Changing the bus connection to the Ethernet connection
FAQ
Changing the bus connection to the Ethernet connection
I want to change the connection type between the GOT2000 series model and Q06HCPU from the one-on-one Q-bus connection to the Ethernet connection.
Which settings for the GOT are required to be changed?
Which settings for the GOT are required to be changed?
Answer
To change the connection type between the GT27 or GT25 model and the Q06HCPU from the one-on-one Q-bus connection to the Ethernet connection, change the following settings in the controller setting on GT Designer3 (GOT2000).
1. Configure the following settings in GT Designer3 (GOT2000).
◆ For GT Designer3 (GOT2000) Version1.100E or later
(1) Select [Common] → [Controller Setting] → [CH1] from the menu.
・ I/F setting
Extend I/F(1st) → Ethernet:Multi
(For GT Designer3 (GOT2000) Version1.170C or later, Standard I/F(Ethernet): Multi)
・ Driver setting
Bus(Q) → Ethernet(MITSUBISHI ELECTRIC), Gateway
(For GT Designer3 (GOT2000) Version1.178L or earlier, Ethernet (MELSEC), Q17nNC, CRnD-700, Gateway)
(2) Select [Common] → [Controller Setting] → [CH1] → [Ethernet Controller Setting] from the menu.
Default values are set. Please change the settings according to the configuration of the connection.
(3) Select [Common] → [GOT Ethernet Setting] → [GOT IP Address Setting] → [Standard Port] from the menu.
(For GT Designer3 (GOT2000) Version1.170C or earlier, select [Common] → [Controller Setting] → [CH1] → [GOT Standard Ethernet Setting] from the menu.)
Please change the settings according to the configuration of the connection.
2. Configure the following settings in GX Works2.
Please configure the settings of the built-in Ethernet port or network parameter according to the configuration of the connection.
For the details, refer to the following.
・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
"5.3 GOT Side Settings"
"5.4 PLC Side Setting"
1. Configure the following settings in GT Designer3 (GOT2000).
◆ For GT Designer3 (GOT2000) Version1.100E or later
(1) Select [Common] → [Controller Setting] → [CH1] from the menu.
・ I/F setting
Extend I/F(1st) → Ethernet:Multi
(For GT Designer3 (GOT2000) Version1.170C or later, Standard I/F(Ethernet): Multi)
・ Driver setting
Bus(Q) → Ethernet(MITSUBISHI ELECTRIC), Gateway
(For GT Designer3 (GOT2000) Version1.178L or earlier, Ethernet (MELSEC), Q17nNC, CRnD-700, Gateway)
(2) Select [Common] → [Controller Setting] → [CH1] → [Ethernet Controller Setting] from the menu.
Default values are set. Please change the settings according to the configuration of the connection.
(3) Select [Common] → [GOT Ethernet Setting] → [GOT IP Address Setting] → [Standard Port] from the menu.
(For GT Designer3 (GOT2000) Version1.170C or earlier, select [Common] → [Controller Setting] → [CH1] → [GOT Standard Ethernet Setting] from the menu.)
Please change the settings according to the configuration of the connection.
2. Configure the following settings in GX Works2.
Please configure the settings of the built-in Ethernet port or network parameter according to the configuration of the connection.
For the details, refer to the following.
・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
"5.3 GOT Side Settings"
"5.4 PLC Side Setting"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (communication)
- Series
- GOT2000 Series