FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Operating the screen with the gesture function while using the SoftGOT-GOT link function
FAQ
Operating the screen with the gesture function while using the SoftGOT-GOT link function
Can I operate the screen of GT SoftGOT2000 with gesture function while using the SoftGOT-GOT link function?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GT SoftGOT > SoftGOT2000
Answer
You cannot operate the screen of the GOT with the gesture function while using the SoftGOT-GOT link function, since GT SoftGOT2000 does not support the gesture function.
If GT SoftGOT2000 obtains the authorization while the GOT is in the screen gesture mode or displays the screen enlarged with a pinch-out operation, the GOT holds the screen gesture mode or display status, and GT SoftGOT2000 displays the normal-sized screen (100%) independently of the display status of the GOT.
After the authorization is transferred to the GOT, switching to the screen gesture mode is enabled on the GOT.
If GT SoftGOT2000 obtains the authorization while the GOT is in the screen gesture mode or displays the screen enlarged with a pinch-out operation, the GOT holds the screen gesture mode or display status, and GT SoftGOT2000 displays the normal-sized screen (100%) independently of the display status of the GOT.
After the authorization is transferred to the GOT, switching to the screen gesture mode is enabled on the GOT.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), SoftGOT
- Series
- GOT2000 Series, SoftGOT