FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Operating the object gesture function
FAQ
Operating the object gesture function
What operations are available for the object gesture function of the GOT2000 series?
Answer
The object gesture function of the GOT2000 series allows the time axis of a graph or document size to be enlarged or reduced with a pinch-in or pinch-out, and a graph or document pages to be scrolled with a swipe or slide.
The object gesture function can be used for the following objects.
・ Historical data list display
・ Alarm display (user)
・ Alarm display (system)
・ Simple alarm display
・ Historical trend graph
・ Document display
・ Video/RGB display object (* Not supported by GT2705-V)
The object gesture function can be used for the following objects.
・ Historical data list display
・ Alarm display (user)
・ Alarm display (system)
・ Simple alarm display
・ Historical trend graph
・ Document display
・ Video/RGB display object (* Not supported by GT2705-V)
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture)
- Series
- GOT2000 Series