FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Specifications of the white model
FAQ
Specifications of the white model
What is the difference between the white model and standard model of GT27and GT25 in addition to the color?
Answer
Differences between the white model and standard model of GT27 and GT25 are as follows.
・ The front face is white-colored.
・ The USB interface is located on the back, and the front face is flat-shaped.
・ The GOT complies with the safety standards (ATEX Directive (*1), KCs Regulation (*1), and UL Class I Division 2).
・ The number and locations of USB hosts (white model: one channel (back), standard model: two channels (front and back))
・ The location of the USB device (white model: one channel (back), standard model: one channel (front))
(*1) The ATEX Directive and KCs Regulation apply only to DC models.
The models that apply to the ATEX Directive or KCs regulation require an optional protective sheet (GT25-□□PSCC-UC) and special fittings (GT25-□□FIT-EXS).
(GT2508-VTWD requires a protective sheet only.)
・ The front face is white-colored.
・ The USB interface is located on the back, and the front face is flat-shaped.
・ The GOT complies with the safety standards (ATEX Directive (*1), KCs Regulation (*1), and UL Class I Division 2).
・ The number and locations of USB hosts (white model: one channel (back), standard model: two channels (front and back))
・ The location of the USB device (white model: one channel (back), standard model: one channel (front))
(*1) The ATEX Directive and KCs Regulation apply only to DC models.
The models that apply to the ATEX Directive or KCs regulation require an optional protective sheet (GT25-□□PSCC-UC) and special fittings (GT25-□□FIT-EXS).
(GT2508-VTWD requires a protective sheet only.)
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT
- Series
- GOT2000 Series