FAQ
FAQAbout Products
- FAQ > Medium-voltage Power Distribution Products > Protection Relays > Protection Relays - MELPRO-A Series > The viewpoint of the instantaneous factor operating characteristics graph
FAQ
The viewpoint of the instantaneous factor operating characteristics graph
What does 100% on the horizontal axis of the instantaneous factor operating characteristics graph mean?
Answer
It means multiples of the settling value. For example, when an instantaneous factor operation settling value of a relay is 30 A, 100% is read as 30 A.
- Product Name
- Protection Relay
- Series
- MELPRO-A Series