FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Communication setting methods when the FX3U-232-BD is used
FAQ
Communication setting methods when the FX3U-232-BD is used
I would like to know the communication setting methods when non-protocol communication is performed using the FX3U-232-BD (for communications with RS-232C).
Answer
The non-protocol communication can be set by the following two methods: (1) setting parameters using a programming tool, such as GX Works2, or (2) writing data to the special data register using a sequence program. (The program created is transferred to a programmable controller.)
A programmable controller operates in the same way regardless of a selected method. If both the methods are executed, the parameter settings are prioritized.
For details, refer to the following.
Section 5 of F. Non-Protocol Communication (RS/RS2 Instruction) in the FX Series Programmable Controllers User's Manual [Data Communication Edition] (Manual number: JY997D16901)
A programmable controller operates in the same way regardless of a selected method. If both the methods are executed, the parameter settings are prioritized.
For details, refer to the following.
Section 5 of F. Non-Protocol Communication (RS/RS2 Instruction) in the FX Series Programmable Controllers User's Manual [Data Communication Edition] (Manual number: JY997D16901)
- Product Name
- FX3U
- Product Category
- Network/Communication, Engineering Software, GX Works2, GX Developer
- Series
- MELSEC-F series