FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > How to use M8029
FAQ
How to use M8029
I would like to know how to use M8029 (Instruction execution complete flag).
Answer
M8029 (Instruction execution complete flag) is shared with multiple instructions.
To obtain an execution completion result of a specific instruction, insert a contact for M8029 directly under the corresponding instruction in a program.
For an example of a program, refer to the following. Section 6.5.2 in the FX3S/FX3G/FX3GC/FX3U/FX3UC Series Programming Controllers Programming Manual [Basic & Applied Instruction Edition]
To obtain an execution completion result of a specific instruction, insert a contact for M8029 directly under the corresponding instruction in a program.
For an example of a program, refer to the following. Section 6.5.2 in the FX3S/FX3G/FX3GC/FX3U/FX3UC Series Programming Controllers Programming Manual [Basic & Applied Instruction Edition]
- Product Name
- FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Product Category
- Main unit, Engineering Software, GX Works2, GX Developer
- Series
- MELSEC-F series