FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Assignment of remote input device and remote output device of FX3U-16CCL-M
FAQ
Assignment of remote input device and remote output device of FX3U-16CCL-M
To use FX3U-16CCL-M CC-link master block, is it possible to assign the remote input device and the remote output device in network parameters?
Answer
The remote input device and the remote output device cannot be assigned in network parameters.
To assign them, create a program for updating data.
To assign them, create a program for updating data.
For details, refer to the following.
Section 8.3 in the FX3U-16CCL-M User's Manual (Manual number: JY997D43601)
The following programmable controllers and GX Works2 support some items, such as mode setting, in network parameters.
FX3G/FX3GC series: Ver. 2.00 or later (GX Works2: Ver. 1.87R or later)
FX3U/FX3UC series: Ver. 3.10 or later (GX Works2: Ver. 1.73B or later)
* The version of programmable controllers can be checked with the last three digits of the data in D8001/D8101.
* When connecting the FX3U-16CCL-M to a programmable controller of the FX3GC/FX3UC series, the FX2NC-CNV-IF or FX3UC-1PS-5V is required.
For details on items which can be set in network parameters, refer to the following.
Section 8.4.1 in the FX3U-16CCL-M User's Manual (Manual number: JY997D43601)
- Product Name
- FX3U-16CCL-M
- Product Category
- Network/Communication, Engineering Software, GX Works2, GX Developer
- Series
- FX3G, FX3GC, FX3U, FX3UC