FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Connection of a totem pole output encoder
FAQ
Connection of a totem pole output encoder
Is it possible to connect a totem pole output encoder to the FX2NC-1HC/ FX2N-1HC/ FX3U-2HC high-speed counters?
Answer
The totem pole output encoder cannot be connected to the FX2NC-1HC/ FX2N-1HC/ FX3U-2HC.
The connectable encoders are as follows.
・ Open collector output type encoder ∙ Differential line driver output type encoder
・ Open collector output type encoder ∙ Differential line driver output type encoder
- Product Name
- MELSEC-F Series
- Product Category
- FX2N, FX2NC, FX3U
- Series
- High-Speed Counting