Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 25232
  • Release Date : 2019/09/02 16:01
  • Print

Regarding USB device

If you remove USB device and then insert it again, the USB device may not work properly (no response).
Category : 

Answer

It occurs on Windows.
The problem (*) that "USB port may stop working after you remove or insert a USB device"
has been reported by Microsoft.
If Windows cannot operate USB devices properly, it is necessary to restart Windows.
If possible, do not connect or disconnect USB devices while Windows is operating.

* For details, refer Microsoft website.
Product Name
MELIPC
Series
MI5000
MI2000
MI1000
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?