Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 37698
  • Release Date : 2020/01/17 17:32
  • Print

Horizontal allowable distance when installing ACB

How much is the allowable flatness of ACB mounting plane?
Category : 

Answer

 Flatness of mounting plane: 1 mm or less. In addition, it is necessary to consider the horizontality of the panel.
Product Name
Low Voltage Air CircuitBreakers
Series
AE-SW
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?