Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • No : 37700
  • Release Date : 2020/01/17 08:58
  • Print

How to connect to 2-pole breaker

N phase connection  to 2-pole breaker?
Category : 

Answer

(1) When "N" is marked on the breaker,connect the N phase wire as marked.   
(2) When "N" is not marked on the breaker, N phase wire can be connected to either pole (left or right).            
 * For 2-pole products with a 3-pole external shape, connect to the left and right poles without using the center pole.
Product Name
Molded Case Circuit Breakers
Series
WS-V

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries