FAQ


FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Low-voltage Circuit Breakers > Molded Case Circuit Breakers > How to connect to 2-pole breaker
FAQ
How to connect to 2-pole breaker
N phase connection to 2-pole breaker?
Answer
(1) When "N" is marked on the breaker,connect the N phase wire as marked.
(2) When "N" is not marked on the breaker, N phase wire can be connected to either pole (left or right).
* For 2-pole products with a 3-pole external shape, connect to the left and right poles without using the center pole.
- Product Name
- Molded Case Circuit Breakers
- Series
- WS-V