FAQ


FAQAbout Products
 - FAQ > Drive Products > Inverters-FREQROL > Connection cable of FR-Configurator
 
FAQ
Connection cable of FR-Configurator
      I want to communicate with FR-Configurator (FR-SW3-SETUP-WJ) using the USB connector. 
Is the Mini-B indicates the standardized Mini-B connector?
  Is the Mini-B indicates the standardized Mini-B connector?
- Category :
 - 
      
- FAQ > Drive Products > Inverters-FREQROL
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
 
 
Answer
    It is the standardized Mini-B connector.
  
    - Product Name
 - Inverter, magnet motor drive
 
- Product Category
 - Inverter
 
- Series
 - FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700