FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > Digit specification for bit devices in ST language with GX Works3
FAQ
Digit specification for bit devices in ST language with GX Works3
I want to create a program in ST language with GX Works3. How can I specify digits for a label of a bit device?
- Category :
Answer
For a label where digits are to be specified, set a bit type array as its data type. The following shows an example of when
a global label is used.
- Global label
- Label name: Lamp
- Data type: Bit array of 16 elements
- Device: Y100
- Program: Describe the digit specification of the bit device for a destination of the MOV instruction.
a global label is used.
- Global label
- Label name: Lamp
- Data type: Bit array of 16 elements
- Device: Y100
- Program: Describe the digit specification of the bit device for a destination of the MOV instruction.
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series
May I have your opinion?
Related FAQ
- Combination of the MELSEC iQ-R series inter-module synchronization function and another network synchronous communication function
- Relay life of the MELSEC iQ-R series relay output module (RY10R2)
- Software to be supplied with GX Works3
- I/O assignment of PLC parameters with GX Works3
- Duplicated coil errors that can be checked with GX Works3