FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > Changing the display language of device comments with GX Works3
FAQ
Changing the display language of device comments with GX Works3
How can I change the display language of device comments with GX Works3?
- Category :
Answer
In the multiple comments display setting, you can set a comment title of the device comments to be set.
<Displaying the multiple comments display setting>
<Displaying the multiple comments display setting>
[View] -> [Mulitple Commnets Dispaly Setting]
<Setting procedure>
(1) Put a checkmark in "Enable Multiple Comments Dispaly".
(2) Put a checkmark in "Available" and enter a comment tile.
(3) Select comments to be displayed in the program editor or various monitor screens in "Target".
(4) Enter a comment in each row in the device comment editor.
Set device comments for each language in the device comment editor.
<Setting device comments>
[Navigation Window] -> [Device] -> [Device Comment]
<Setting procedure>
(1) Put a checkmark in "Enable Multiple Comments Dispaly".
(2) Put a checkmark in "Available" and enter a comment tile.
(3) Select comments to be displayed in the program editor or various monitor screens in "Target".
(4) Enter a comment in each row in the device comment editor.
Set device comments for each language in the device comment editor.
<Setting device comments>
[Navigation Window] -> [Device] -> [Device Comment]
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series
May I have your opinion?
Related FAQ
- Language selection function of GX Works2
- Combination of the MELSEC iQ-R series inter-module synchronization function and another network synchronous communication function
- Digit specification for bit devices in ST language with GX Works3
- Using a commercially-available SD memory card for a MELSEC iQ-R series CPU module
- Models of extended SRAM cassettes that can be used with MELSEC iQ-R series CPU modules