FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > Combination of the MELSEC iQ-R series inter-module synchronization function and another network synchronous communication function
FAQ
Combination of the MELSEC iQ-R series inter-module synchronization function and another network synchronous communication function
Can I use the MELSEC iQ-R series inter-module synchronization function together with another network synchronous communication function, such as the CC-Link IE Field Network synchronous communication function?
- Category :
Answer
You can use the MELSEC iQ-R series inter-module synchronization function together with the CC-Link IE Field Network
synchronous communication function.With the CC-Link IE Field Network synchronous communication function,
you can operate other slave stations connected in the same network synchronously in an inter-module synchronization
cycle of the MELSEC iQ-R series inter-module synchronization function.
synchronous communication function.With the CC-Link IE Field Network synchronous communication function,
you can operate other slave stations connected in the same network synchronously in an inter-module synchronization
cycle of the MELSEC iQ-R series inter-module synchronization function.
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series
May I have your opinion?
Related FAQ
- Relay life of the MELSEC iQ-R series relay output module (RY10R2)
- Software to be supplied with GX Works3
- Using Q series terminal blocks and connectors with MELSEC iQ-R series modules
- Overhead time of when a fixed scan execution type program of the MELSEC iQ-R series CPU module is executed
- Models of extended SRAM cassettes that can be used with MELSEC iQ-R series CPU modules