Start main contents
Font Size
S
M
L
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC iQ-R Series
>
Overhead time of when a fixed scan ex...
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
No : 22465
Release Date : 2018/09/03 17:28
Update : 2018/09/19 11:57
Print
Overhead time of when a fixed scan execution type program of the MELSEC iQ-R series CPU module is executed
How long is the overhead time of when a fixed scan execution type program of the MELSEC iQ-R series CPU module?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC iQ-R Series
Answer
When the block number of the file register (R) is saved and stored, the overhead time becomes 35.9 [us].
When the number of the file register is not saved or stored, the overhead time becomes 18.6 [us].
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
Models of batteries that can be used ...
Mounting Q series modules on a MELSEC...
I/O numbers of a MELSEC iQ-R series I...
The number of times to insert and rem...
Software to be supplied with GX Works3
page top
HOME
FAQ