Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22473
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/21 16:38
  • Print

OS compatible with GX Works3

Which OS is compatible with GX Works3?
Category : 

Answer

GX Works3 is compatible with the following OSs. (As of Sep,2018)

- Microsoft Windows 10
- Microsoft Windows 8.1
- Microsoft Windows 8
- Microsoft Windows 7
- Microsoft Windows Vista *
- Microsoft Windows XP *

(* GX Works3 is not compatible with Windows XP or Windows Vista of 64-bit version.)
Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?