FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Heat generation of Q61P power supply module
FAQ
Heat generation of Q61P power supply module
How much heat is generated from a Q61P power supply module?
- Category :
Answer
Since the conversion efficiency of the power supply module is approximately 70%, and 30% of the output power is dissipated as heat, the power consumption is 3/7 of the output power. For more details of the calculation formula, refer to the following manual.
- QCPU User's Manual (Hardware Design, Maintenance and Inspection) Appendix 9
- QCPU User's Manual (Hardware Design, Maintenance and Inspection) Appendix 9
- Product Name
- MELSEC-Q Series
- Series
- Q (Q mode)