Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22534
  • Release Date : 2018/09/03 17:28
  • Print

Duplicated coil error

The duplicated coil error is detected when program check is executed.
Is this error detected when SET instruction and RST instruction use the same device?
Category : 

Answer

The duplicated coil error is detected when SET instruction and RST instruction use the same device.
Product Name
MELSEC-Q Series
Series
Software Package (GPP function)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?