Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22535
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/20 14:46
  • Print

Error code "2401" in QCPU

The error code "2401" has occurred in QCPU.
The Parameter No. under Individual Error Information is "1100H". Are there any remedies?
Category : 

Answer

The error code "2401" is "FILE SET ERROR".
The individual information parameter number "1100H" corresponds to a file register.
The cause of the error is that the file register file specified by the parameter cannot be created.
Check the amount of free space of the memory in which the file register file is created.
Product Name
MELSEC-Q Series
Series
Q (Q mode)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?