Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22586
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/20 17:33
  • Print

Communication between built-in Ethernet port QCPU modules

Which communication methods are available between built-in Ethernet port QCPU modules?
Category : 

Answer

The following communication methods are available between built-in Ethernet port QCPU modules.

- Socket communications are possible.
- Communications equivalent to READ/WRITE instructions, which are data link instructions, are achieved by using FB libraries 
  for data link in MELSOFT Library.
Product Name
MELSEC-Q Series
Series
Q (Q mode)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?