Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22603
  • Release Date : 2018/09/03 17:29
  • Print

Label programs in GX Works2

Can a label program be changed to an unlabeled program in GX Works2?
Category : 

Answer

Change the program using the following method.

Write the label program to the programmable controller CPU and perform PLC read for the parameters and the program without selecting symbolic information in the Read from PLC window.
Product Name
MELSEC-Q Series
Series
Software Package (GPP function)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?