FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Fixed scan execution type (program setting item)
FAQ
Fixed scan execution type (program setting item)
As one of the program setting items, "Fixed Scan" (fixed scan execution type) can be selected. What type of program is it?
- Category :
Answer
A fixed scan execution type program is a program executed at specified time intervals. This type of programs, unlike interrupt programs, can be interrupted in units of files without interrupt pointers or the IRET instruction.
For more details, refer to the following.
SH-080808ENG Qn(H)/QnPH/QnPRHCPU User's Manual(Function Explanation, Program Fundamentals)
2.3.5 Fixed scan execution type program
For more details, refer to the following.
SH-080808ENG Qn(H)/QnPH/QnPRHCPU User's Manual(Function Explanation, Program Fundamentals)
2.3.5 Fixed scan execution type program
- Product Name
- MELSEC-Q Series
- Series
- Q (Q mode)