Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22626
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/21 10:36
  • Print

The VxWorks simulator CW-SIM

What does the software CW-SIM deal with?
Category : 

Answer

CW-SIM is a simulation software that allows a VxWorks program to be executed on a personal computer without a
C Controller module. There are two types of CW-Sim simulation environments.

 - CW-Sim (license product: SW1DNC-CWSIM-E, additional product: SW1DNC-CWSIM-EZ)
    Programs can be debugged on a personal computer on which CW Workbench is installed.
 - CW-Sim Standalone (SW1DNC-CWSIMSA-E)
    Programs can be executed on a personal computer whether or not CW Workbench is installed on the computer.
 - Single step executions (line debugging) are impossible.
Product Name
MELSEC-Q Series
Series
C Language Controller
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?