FAQ


FAQAbout Products
 
 - FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Whether or not totem pole output type encoders are connected
FAQ
Whether or not totem pole output type encoders are connected
      Is it possible to connect a totem pole output type encoder to the high-speed counter module QD62?
    
  - Category :
Answer
    Totem pole output encoders cannot be connected to QD62.
The following types of encoders can be connected.
- Open collector output type encoders
- CMOS level voltage output type encoders
    The following types of encoders can be connected.
- Open collector output type encoders
- CMOS level voltage output type encoders
- Product Name
- MELSEC-Q Series
- Series
- High Speed Counter Module