Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22645
  • Release Date : 2018/09/03 17:29
  • Print

Accessing file registers from the built-in Ethernet port QCPU using A-compatible 1E frames

Is it possible to access file registers from the built-in Ethernet port QCPU using the MC protocol's A-compatible 1E frames?
Category : 

Answer

The QnUDE(H)CPU modules with serial numbers with upper 5 digits of "14112" or later indicate compatibility with the function. The accessible device range is from R0 to R8191. The High-speed Universal model QCPU (QnUDVCPU) does not support the function.
Product Name
MELSEC-Q Series
Series
Q (Q mode)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?