Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22648
  • Release Date : 2018/09/03 17:29
  • Print

Open setting of the built-in Ethernet port QCPU

When all the 16 ports are configured to use socket communication, is it possible to communicate with GX Developer or GX Works2 through the Ethernet?
Category : 

Answer

No.
It is necessary to configure one port to use the MELSOFT connection.
Product Name
MELSEC-Q Series
Series
CPU
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?