FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Clock function accuracy
FAQ
Clock function accuracy
What does the following information on the basic model QCPU's clock function denote?
- Accuracy: -2.57 to +5.27s(TYP.+2.22s)/d at 25 degrees Celsius.
- Accuracy: -2.57 to +5.27s(TYP.+2.22s)/d at 25 degrees Celsius.
- Category :
Answer
It means that in an ambient temperature of 25 degrees Celsius, an error per day falls within the range of "delay of 2.57s" to "advance of 5.27s".
"TYP.+2.22s" denotes that the standard value is "advance of 5.27s".
"TYP.+2.22s" denotes that the standard value is "advance of 5.27s".
- Product Name
- MELSEC-Q Series
- Series
- CPU