Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22661
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/21 12:18
  • Print

Print settings of the device list in GX Works2

In GX Works2, the device list printed from the Print window does not list devices used. Why does this occur?
Category : 

Answer

When [Display Option] -> [Used devices] -> [Contact] and [Coil] are selected in the Device List window,
devices used are not displayed.
Product Name
MELSEC-Q Series
Series
Software Package (GPP function)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?