Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22680
  • Release Date : 2018/09/03 17:29
  • Print

Parameter settings required to use the MODBUS(R) interface module as a slave station

Is it necessary to set parameters when the MODBUS(R) interface module QJ71MB91/QJ71MT91 is used as a slave station?
Category : 

Answer

If preset initial values are used, parameters do not need setting.
If changing the basic parameter or MODBUS(R) device assignment parameter, use a sequence program, GX Works2, or GX Configurator-MB to change it.
Product Name
MELSEC-Q Series
Series
MODBUS

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries