Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22690
  • Release Date : 2018/09/03 17:29
  • Print

Cables connected to the Ethernet port on the universal model QCPU

Which type of cable should I use for a connection to the Ethernet port on a universal model QCPU module, straight cable or cross cable?
Category : 

Answer

If a direct connection is made, either type can be used.
If making a connection via a hub, use a straight cable.
Product Name
MELSEC-Q Series
Series
Q (Q mode)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?